REGEN.VOLTSLOW
Description
This parameter returns the DC bus voltage at which the regen circuit begins to dissipate power. When VBUS.VALUE is above REGEN.VOLTSLOW, the regen circuit is off. When VBUS.VALUE is between REGEN.VOLTSLOW and REGEN.VOLTSHIGH, the regen control commands a duty cycle computed from the bus voltage level.
The drive recalculates REGEN.VOLTSLOW when VBUS.ACNOMINAL changes (or VBUS.DCNOMINAL when VBUS.DCOPERATION = 1).
Examples
Usage
The drive configures the REGEN.VOLTSLOW parameter based on power board ratings and the and value of REGEN.VOLTSLOW is automatically set when the value of VBUS.ACNOMINAL is changed.
| VBUS.ACNOMINAL | REGEN.VOLTSLOW | |
|---|---|---|
| Medium Voltage (MV) | 240 | 380 |
| High Voltage (HV) | 480 | 760 |
Context
For more information on DC bus operation and regeneration, refer to Power View and Regeneration.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-09-02-000 |
General Information
|
Type |
Read Only |
|
Units |
VDC |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
REGEN.VOLTSLOW |
3007h |
11h |
Unsigned16 |
- |
- |
Read only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2416 |
1 |
2416 (0x970) |
REGEN.VOLTSLOW |
Unsigned16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.VOLTSLOW |
2416 |
Unsigned16 |
Read Only |
- |